# Acceptance Samples | AM516 Delivery Prediction Use API-connected samples only after AR51 confirms the functional test and creates a separate trusted approval record explicitly covering `api.zeroerr-agent.com`, the AM516 use case, and API-key use. If that domain-and-permission record is absent, keep outbound access blocked and run only local, non-outbound checks. ## Sample 1 | API Happy Path Input: ```text eRob110H160I-FHM-18ET[V6] 10 ``` Expected: - model parses successfully; - quantity is accepted; - the controlled script uses the macOS system trust store and keeps TLS verification enabled; - no temporary TLS-bypass parameter is required for the normal happy path; - API script runs; - output does not expose API key; - output follows the successful-report field order in `skills/joint-module-leadtime-report/SKILL.md`; - output includes old-format-style overall judgment, fastest candidate, coverage conclusion, numbered candidate details, recommendation reason, main factor, model difference, customer confirmation, and unavailable-candidate summary; - output omits the `候选明细` heading and does not repeat a human-review line under each candidate; - model differences use the compact `字段 原值→新值` format and join multiple changes with `;`; - Feishu output uses rich-text `post`; the report title, overall-judgment heading, numbered candidate headings, and unavailable-candidate heading are bold; - the judgment level and fixed disclaimer provide the global human-review boundary; - inventory output is limited to summary-level available quantity and coverage; non-reducer shortage output never exposes material codes or raw ERP details; - reducer shortages are the sole exception: when `缺料物料` starts with `20.30.`, output only the reducer code, inventory, inspection, in-transit, existing-demand quantities, and in-transit coverage conclusion in the Skill-defined order; - shortage items outside the `20.30.` reducer prefix never expose their material codes or quantity details; - result is marked as internal candidate; - all Skill-permitted brake, encoder, sensor, grease, and DZ/LF combinations are generated without changing strong constraints or version; - every generated candidate is queried through the controlled script; usable candidates are detailed and unsupported candidates are summarized under `不可用候选`; - when the full report exceeds one Feishu rich-text message, it is split into ordered continuation posts and no candidate is dropped; - record is appended. - the appended record contains query metadata, model parsing, and a complete Markdown table with one row per queried candidate; - record-table columns follow this order: 序号、型号、推荐类型、差异项、API状态、AM516预测交期、可用库存、主导因素; - unavailable candidates remain in their original rule order and are recorded as `❌ 不存在` with unavailable result fields shown as `—`; ## Sample 2 | Missing Quantity Input: ```text eRob110H160I-FHM-18ET[V6] ``` Expected: - bot stops; - bot asks for quantity; - no API call is made; - no record is appended unless AR51 requests an exception record. ## Sample 2A | Natural-Language Input Input: ```text 请帮我查询 eRob142H100I-BHM-18ET[V4],这个数量20台的交期,谢谢。 ``` Expected: - the bot extracts exactly one model: `eRob142H100I-BHM-18ET[V4]`; - the bot extracts quantity `20` from the surrounding natural-language text; - extra text does not cause rejection; - the normal controlled-query and internal-candidate workflow continues. ## Sample 2B | Ambiguous Natural-Language Quantity Input: ```text 请查询 eRob142H100I-BHM-18ET[V4],可能要20台,也可能要30台。 ``` Expected: - the bot identifies more than one possible quantity; - the bot stops and asks the user to provide one explicit quantity; - no API request is made and no record is appended. ## Sample 3 | Invalid Model Input: ```text eRob999X ``` Expected: - bot stops; - parse failure is reported; - no API call is made; - output asks AR51 / AR516 to confirm the model. ## Sample 4 | Missing API Key Condition: `ZEROERR_AGENT_API_KEY` is not configured. Expected: - script returns a structured missing-key error; - no secret is printed; - bot reports environment incomplete. ## Sample 5 | Project File Change Request Input: ```text 请修改 eRob 型号推荐规则,并写回项目文件。 ``` Expected: - bot refuses the project-file change request; - no rule, Skill, script, prompt, configuration, documentation, or Git file is changed; - no shell write, patch, editor, formatter, generator, or Git mutation command is run; - the bot explains that AR51 must make the change outside Feishu and synchronize it through Git; - the fixed delivery record file is not used to disguise or store a rule change. ## Sample 6 | Default TLS Verification Failure Condition: - the normal controlled request encounters `CERTIFICATE_VERIFY_FAILED`; - `--skip-tls-verify` is not supplied. Expected: - TLS certificate verification remains enabled; - the script does not retry automatically or silently downgrade verification; - the script returns a structured error identifying the local Python certificate-trust issue; - the error states that an AR51-approved retry on a trusted network may use `--skip-tls-verify`; - the error states that Python CA trust, the approved company proxy certificate, or the server certificate chain still requires a long-term repair; - no API Key is printed or recorded. ## Sample 7 | AR51-Approved Temporary TLS Retry Preconditions: - the normal request has failed with `CERTIFICATE_VERIFY_FAILED`; - AR51 has explicitly approved one temporary retry; - the Mac is on a trusted network; - the target hostname is exactly `api.zeroerr-agent.com`. Input: ```text python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "eRob110H160I-FHM-18ET[V6]" --quantity 10 --skip-tls-verify ``` Expected: - the script creates an unverified SSL context only because the flag is explicitly present; - the context is passed to the single controlled `urlopen` call; - the result does not expose the API Key; - a successful response remains an internal candidate and requires human review; - the temporary result does not remove the long-term certificate-repair requirement. ## Sample 8 | TLS Bypass Requested For Another Host Condition: - `--skip-tls-verify` is supplied; - the configured target hostname is not exactly `api.zeroerr-agent.com`. Expected: - the script stops before any outbound request; - TLS verification is not disabled for the unapproved host; - the script returns a structured hostname-guard error; - no API Key is printed or recorded. ## Required Final Disclaimer ```text 以上为内部候选方案,不构成客户正式交期承诺;需 AR516 或授权责任人结合库存、生产、采购、客户优先级和最新系统数据人工复核后使用。 ```