# Deployment Checklist | AM516 Delivery Prediction ## 1. Account And Device - [ ] Department shared Mac is confirmed as the runtime device. - [ ] Device owner and reboot owner are confirmed. - [ ] Department email is confirmed. - [ ] Department ChatGPT / Codex account plan is confirmed. - [ ] Account ownership, password custody, and handover method are confirmed. - [ ] Screen lock, disk encryption, and remote management requirements are confirmed by AR51. ## 2. Git And Project - [ ] `AM516_Feishu_Bot` is available on the shared Mac. - [ ] Git remote, branch, update, and rollback mechanisms are constructed by TH8. - [ ] TH8 is the supporting IT department, but its project responsibility is limited to Git construction and excludes AM516 rules, functional implementation, network access, account permissions, secrets, and outbound approval. - [ ] Branch and update method are confirmed. - [ ] Mac Studio Codex has project write permission for AR51-assigned work through direct non-Feishu local entry points, including Codex automations or scheduled tasks and the required Git operations. - [ ] The Feishu runtime account has read-only access to the project tree except append access to `records/delivery_prediction_records.md` and approved non-project log storage. - [ ] Project edits through Feishu are prohibited without exception; AR51-authorized rule and function changes are made outside Feishu and synchronized through Git. - [ ] Permission checks distinguish the request entry point: Feishu requests do not inherit local Codex write permission even when Codex is the underlying executor. - [ ] Rollback method is confirmed. ## 3. Secrets - [ ] AR51 has approved the API-key purpose, storage, use, rotation, and revocation method in a traceable record. - [ ] `ZEROERR_AGENT_API_KEY` is configured without printing or committing it. - [ ] `.env` or local secret file is excluded by `.gitignore`. - [ ] No API key appears in Markdown, logs, Feishu output, or Git history. ## 4. Runtime - [ ] Python 3 is available. - [ ] The controlled script can run locally. - [ ] AR51 has created a trusted approval record explicitly covering outbound access to `api.zeroerr-agent.com`, the AM516 use case, and API-key use. - [ ] If that domain-and-permission record is absent, outbound access remains blocked; a general AR51 functional-test approval is not sufficient by itself. - [ ] Only after approval is recorded, network can reach the AR836 delivery prediction API. - [ ] Feishu bot bridge or local entry is configured. - [ ] The Feishu app has `im:message.reactions:write_only` so the bot can add the `OnIt` received reaction to valid query messages. - [ ] Logs are stored outside Git or in an approved non-secret location. ## 5. Acceptance - [ ] AR51 confirms that AM516 rules, functional design, implementation, validation, iteration, network access, account permissions, secrets, and outbound approval are owned by AR51, not TH8. - [ ] After the approval gate is satisfied, at least one valid model + quantity query succeeds; otherwise the blocked outbound state is recorded without attempting the request. - [ ] Missing API key returns a structured error without leaking secrets. - [ ] Missing, invalid, multiple, or ambiguous model/quantity input stays silent and makes no API call or record append. - [ ] The initial response queries no more than four recommended candidates in addition to the original-model baseline; same-sender, same-chat continuation queries the next four without duplication. - [ ] Candidate continuation without matching active context stays silent; a bridge restart or six-hour expiry requires the complete model and quantity again. - [ ] Output includes the fixed internal-candidate disclaimer. - [ ] A real valid query shows the `OnIt` typing reaction below the original message rather than creating a reply bubble or reply thread. - [ ] Records append to `records/delivery_prediction_records.md`. - [ ] A direct AR51 task in Mac Studio Codex can modify a test project file or perform the intended Git update without being blocked by the Feishu read-only rule. - [ ] A Feishu request to modify a rule or other project file is refused and leaves all project files unchanged.