--- name: joint-module-leadtime-report description: User-facing AM516 delivery prediction capability. Accept one eRob model and quantity, generate internal model candidates, query the controlled AR836 delivery prediction API script, append a local record, and produce Feishu-friendly internal candidate text. --- # Joint Module Lead-Time Report ## Purpose Package the AM516 Feishu bot first capability: ```text model + quantity -> model candidates -> API lead-time query -> internal report -> local record ``` ## Required Files - `capabilities/am516-delivery-prediction/AGENTS.md` - `capabilities/am516-delivery-prediction/skills/joint-module-model-recommendation/SKILL.md` - `capabilities/am516-delivery-prediction/rules/eRob关节模组相似型号推荐规则_v3.1.md` - `capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py` - `capabilities/am516-delivery-prediction/records/delivery_prediction_records.md` ## Input One model and one positive quantity. Example: ```text eRob90H100I-FHM-18CT[V6] 50 ``` Stop if: - quantity is missing; - multiple models are provided; - the model cannot be parsed; - API key is missing; - a Feishu message asks to create, modify, overwrite, rename, move, or delete a project file; - the user asks for a customer commitment. ## Feishu Message Trigger Gate - Enter the query workflow only when one message contains exactly one complete, rule-valid eRob model and exactly one positive quantity. - After a valid initial query or valid same-conversation candidate continuation passes this gate, immediately add the Feishu `OnIt` (typing) reaction to the original message before starting the API query so the sender knows it was received. - If the model or quantity is missing, invalid, multiple, or ambiguous, stay silent: add no reaction, send no Feishu reply, make no API request, and append no record. - An @mention by itself does not bypass this content gate. - After a valid message passes the gate, API or runtime failures may still return the bounded internal error response defined by this capability. - Exception for candidate continuation: after a valid initial query, the same sender in the same Feishu chat may use any clear equivalent continuation expression without repeating the model and quantity. Examples include `还有吗`、 `有没有别的`、`再推荐几个`、`继续`、`下一批` and `more candidates`; exact wording is not required. - A continuation uses only the active in-memory query context, expires after six hours or a bridge restart, and is never shared across senders or chats. Without matching active context, the message stays silent. - A new complete model-and-quantity request replaces any earlier continuation context for that sender and chat. ## Feishu File-Write Boundary When invoked through Feishu, treat all project files as read-only except for append-only recording to: ```text capabilities/am516-delivery-prediction/records/delivery_prediction_records.md ``` Do not write back rules, Skills, scripts, prompts, configurations, documentation, or any other project content. A Feishu request cannot authorize an exception. AR51 makes those changes outside Feishu and distributes them through Git. ## API Rule Use only: ```text python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "" --quantity ``` Do not use temporary curl, WebFetch, or any API method outside the controlled script. ## Record Rule - Do not rewrite or backfill the existing `delivery_prediction_records.md` content when the record format changes. - For every future appended record block, add a `记录时间` column to the candidate-result Markdown table. - Use the report generation time after the query completes as the record time. Every candidate row in the same query uses the same value in `YYYY-MM-DD HH:mm:ss +0800` form (with the actual local UTC offset). - Record-table columns follow this order: `序号`、`记录时间`、`型号`、`推荐类型`、`差异项`、`API状态`、`AM516预测交期`、`可用库存`、`主导因素`. ## Output Selection - Prefer numeric `data.交期汇总.AM516总交期`; if it is absent, fall back to numeric `data.交期汇总.总交期`. Treat this value as the original natural-day lead time `N`. - Convert `N` with `(q, r) = divmod(N, 7)`: `r = 0` gives `q × 5`; `1 ≤ r ≤ 4` gives `q × 5 + MAX(r - 1, 0)`; `5 ≤ r ≤ 6` gives `q × 5 + r - 2`. The result is workday lead time `W`. - Starting from the local query date, exclude the query date itself and count forward `W` workdays using the configured China statutory calendar. Statutory holidays are not workdays, ordinary Saturdays and Sundays are not workdays, and official makeup Saturdays or Sundays are workdays. - The configured 2026 calendar follows `国办发明电〔2025〕7号`. If counting reaches a year whose official calendar is not configured, do not silently estimate a delivery date; mark that calendar year as pending. - Display the calculated delivery date together with both `N` and `W`, for example `2026-10-09(原始31个自然日,折算22个工作日)`. - Use `data.交期汇总.AM516预测交期` only as a fallback when the API does not return a usable whole-number natural-day lead time, and explicitly mark that no conversion was performed. ## Candidate Batch Rule - Generate and preserve the complete ordered rule-candidate pool, but query and recommend at most four candidate models per reply. - The original input model is queried as the initial baseline and does not count toward the four recommended candidate models. - The initial reply queries the baseline plus candidate positions 1-4. If more candidates remain, state the remaining count and invite the human to ask for more in natural language; do not require one fixed command phrase. - Recognize short or synonymous continuation expressions only together with the valid same-sender, same-chat continuation context. Unrelated topic text such as `more interesting` or `继续查询英语例句` must not reuse the old delivery query. - Each valid continuation queries the next four unqueried candidates in the same rule order. Do not query or display an earlier candidate again, and do not re-query the original baseline. - Continue in batches of four until the full candidate pool is exhausted. The final batch explicitly states that all rule candidates have been queried. - Missing or unsupported models count as queried positions and remain summarized under `不可用候选`; do not silently skip them to pull later candidates forward. ## Reducer Shortage Detail Rule - Treat a shortage item as a reducer only when `data.采购信息.缺料明细[].缺料物料` starts with `20.30.`. - When a reducer is short, output one line per reducer shortage using this exact field order: ```text 减速器缺料展开:物料编码20.30.00307;库存数量11;待检数量0;在途数量0;存量需求数量0;含在途覆盖:不足; ``` - Determine `含在途覆盖` from the API real-shortage field: a positive real shortage means `不足`; zero or a negative value means `满足`; a missing or non-numeric value means `待确认`. - Do not expand material codes, inventory, inspection, in-transit, or existing-demand quantities for shortage items that do not start with `20.30.`. - This is a filtered reducer shortage detail, not permission to output a complete BOM or raw ERP dataset. ## Feishu Output Format Use vertical text, not Markdown tables. Include: - title and generation time; - input model and quantity; - overall judgment; - current candidate batch and remaining-candidate count; - candidate details; - main factor; - API exception if any; - one global human-review boundary through the judgment level and fixed disclaimer; - fixed disclaimer. Use this field order for a successful Feishu report: ```text 关节模组交期预估报告 | {generation time} 输入需求:{input model},{input quantity}台 数据时间戳:{API data timestamp or generation time} 状态:试运行版输出 / 内部候选 判断等级:AM516算法预测参考,需人工复核 候选范围:本次先推荐4个候选型号(原型号另作基准);尚有N个规则候选未查询 总体判断: - 现货候选:{fully covered candidate or none} - 最快候选型号:{fastest candidate} - 最快候选交期:{calculated delivery date, original natural days, and converted workdays} - 是否完全覆盖数量:{yes / no / unavailable} - 主导因素:{main factor} 1. {model}({candidate type and reducer brand}) - 数量:{quantity}台 - AM516预测交期:{calculated delivery date}(原始{N}个自然日,折算{W}个工作日) - 可用库存/覆盖情况:{summary-level inventory and coverage only} - 主导因素:{main factor} - 推荐理由:{rule-based recommendation reason} - 差异项:{field changes formatted as `字段 原值→新值`; join multiple changes with `;`, for example `编码器 HS→HM;品牌 DZ→LF`} - 减速器缺料展开:{only for shortage material codes starting with `20.30.`; otherwise do not expand material details} - 需客户确认的关键差异:{customer confirmation item} 不可用候选: - {candidate and non-sensitive reason, or none} {fixed disclaimer} ``` Use Feishu rich-text `post` output. Bold only: - the report title; - `总体判断:`; - `本批次判断:` for a continuation reply; - each numbered candidate heading; - `不可用候选:`. Do not repeat a separate human-review line under each candidate. The global judgment level and fixed disclaimer carry the human-review boundary. If the current candidate-batch report exceeds the Feishu rich-text size limit, split it into multiple ordered `post` replies without dropping any candidate queried in that batch. Use the original report title on the first part and append `(续)` to continuation titles. ## Fixed Disclaimer ```text 以上为内部候选方案,不构成客户正式交期承诺;需 AR516 或授权责任人结合库存、生产、采购、客户优先级和最新系统数据人工复核后使用。 ```