# Runbook | AM516 Delivery Prediction ## Normal Query 1. Extract exactly one model and one positive quantity from the compact input or natural-language message; stop if either field is missing or ambiguous. 2. Read the capability `AGENTS.md`. 3. Confirm AR51 has approved the functional test. 4. Confirm a separate trusted AR51 approval record explicitly covers `api.zeroerr-agent.com`, the AM516 use case, and API-key use. 5. If that domain-and-permission record is absent, stop before any outbound request; a general functional-test approval is insufficient by itself. 6. Use model recommendation rules to generate internal candidates. 7. Run the controlled script for the original model and approved candidates. 8. Summarize the internal candidate result. 9. Append a non-secret record. 10. Return Feishu-friendly text with the fixed disclaimer. ## Approved Script ```text python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "" --quantity ``` ## Environment Check ```text python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "eRob110H160I-FHM-18ET[V6]" --quantity 10 ``` Do not run this check until AR51 confirms the functional test and creates a separate trusted approval record explicitly covering `api.zeroerr-agent.com`, the AM516 use case, and API-key use. ## Normal TLS Trust Configuration The controlled query script injects `truststore` before making the request. Normal queries therefore keep TLS certificate verification enabled while using the macOS system trust store, including an AR51-approved company proxy root certificate installed and trusted in the system keychain. The shared Mac runtime must keep `truststore` installed through `requirements.txt`. If normal verification still fails, AR51 must verify that the required company proxy root certificate is installed and trusted in macOS, or arrange repair of the service certificate chain. Do not make `--skip-tls-verify` the normal operating mode. ## Temporary TLS Certificate Workaround Normal requests must keep TLS certificate verification enabled. The controlled script does not automatically retry or silently downgrade TLS verification. Only when all of the following conditions are met may AR51 authorize one controlled retry with `--skip-tls-verify`: 1. the normal controlled request failed with `CERTIFICATE_VERIFY_FAILED`; 2. AR51 explicitly approved the temporary retry; 3. the Mac is connected to a trusted network; 4. the target hostname is exactly `api.zeroerr-agent.com`. Approved one-time retry command: ```text python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "eRob110H160I-FHM-18ET[V6]" --quantity 10 --skip-tls-verify ``` The script refuses to skip TLS verification for any other hostname. This option is a temporary validation measure only; AR51 must still arrange the long-term repair of the Python CA trust, approved company proxy certificate, or server certificate chain. Never place the API Key in the command line, Markdown, logs, or output. ## Error Handling | Error | Action | |---|---| | Missing model | Ask for one model | | Multiple models | Ask AR51 to split queries | | Missing quantity | Ask for quantity | | Multiple possible quantities | Ask the user to state one quantity explicitly, for example `数量20台` | | Invalid model | Stop and report parse failure | | Missing trusted AR51 domain-and-permission approval record | Stop before the API request; report that a general functional-test approval does not automatically approve a specific outbound domain | | Missing API key | Stop and report environment incomplete | | `CERTIFICATE_VERIFY_FAILED` | Return the structured local certificate-trust error; use `--skip-tls-verify` only for one AR51-approved retry on a trusted network and only for `api.zeroerr-agent.com` | | `--skip-tls-verify` with any other hostname | Stop before the request; do not disable TLS verification | | API error | Report API error summary without raw sensitive data | | Customer commitment request | Stop and route to AR51 / AR516 / TH1 | ## Maintenance - AM516 rules, functional design, implementation, validation, iteration, network access, account permissions, secrets, and outbound approval are owned by AR51. - TH8 is the supporting IT department but is responsible only for Git repository and synchronization-mechanism construction in this project. - Feishu handling is read/output/record-only. It may append only to `records/delivery_prediction_records.md` and must not mutate any other project file. - A Feishu request cannot authorize a rule, Skill, script, prompt, configuration, documentation, or Git change. - AR51 makes rule and function changes outside Feishu; the shared Mac receives them through the TH8-built Git synchronization mechanism.