--- name: joint-module-model-recommendation description: Parse one eRob robot joint module model and generate internal similar-model candidates from the packaged v3.1 recommendation rule source. This skill does not query inventory, ERP, production, purchasing, lead-time, or customer commitment data. --- # Joint Module Model Recommendation ## Purpose Generate internal similar-model candidates for one eRob joint module model. ## Rule Source Use the packaged local rule file: ```text capabilities/am516-delivery-prediction/rules/eRob关节模组相似型号推荐规则_v3.1.md ``` If the rule file is missing, stop. ## Boundary - Output is internal candidate only. - Do not query API, ERP, inventory, purchasing, production, or lead-time data. - Do not write "can directly replace", "committed", or "can deliver". - The original model is the baseline. - Candidates require customer confirmation and AR516 or authorized human review. ## Input Accept one model only. Example: ```text eRob90H100I-FHM-18CT[V6] ``` ## Core Constraints Strong constraints must stay unchanged: - outer diameter; - gear ratio; - installation; - communication; - output shaft. Allowed upgrades: - brake `F -> B`; - encoder upgrade only, never downgrade; - sensor `N -> T`; - standard grease to low-temperature grease; - DZ and LF brand may be candidates. ## Full Candidate Generation - Keep outer diameter, structure, gear ratio, installation, communication, output shaft, and version unchanged. - Generate the full Cartesian set across every allowed value for brake, encoder, sensor, grease, and DZ/LF brand. - Encoder options are directional: `S -> M/HS/HM`, `M -> HS/HM`, `HS -> HM`, and `HM` has no further automatic upgrade. - Include the original model separately as the baseline and deduplicate all generated models. - Never generate a brake, encoder, sensor, or grease downgrade. - Preserve the complete deduplicated candidate pool in rule order so the lead-time capability can page through it deterministically. - The original model is a baseline and does not count toward the four recommended candidate models in a batch. - When used by the lead-time capability, pass only the first four candidates on the initial query. A same-conversation human request for more candidates passes the next four, without repeating or reordering earlier candidates. - This recommendation Skill does not call the delivery-prediction API itself. The lead-time capability queries only the current candidate batch and summarizes missing or unsupported models under `不可用候选`. ## Output Use a vertical list with: - model; - candidate type; - difference; - recommendation reason; - customer confirmation item; - human review item. Format the difference field as `字段 原值→新值`. Join multiple changes with the Chinese semicolon `;`, for example: ```text 差异项:编码器 HS→HM;品牌 DZ→LF ```