Files
AM516/shared/runtime/install_material_name_refresh.py

68 lines
2.9 KiB
Python
Raw Permalink Blame History

This file contains ambiguous Unicode characters
This file contains Unicode characters that might be confused with other characters. If you think that this is intentional, you can safely ignore this warning. Use the Escape button to reveal them.
"""Install the native macOS background material-name refresher."""
from __future__ import annotations
import argparse
import os
import plistlib
import subprocess
import sys
from pathlib import Path
PROJECT_ROOT = Path(__file__).resolve().parents[2]
LABEL = "com.am516.material-name-refresh"
def launch_agent(project: Path, python: Path, log_dir: Path, client: Path | None = None) -> dict:
command = [str(python), str(project / "capabilities/am516-delivery-prediction/scripts/refresh_material_names.py"), "--due", "--interval-hours", "48"]
if client is not None:
command.extend(["--kingdee-client", str(client)])
return {
"Label": LABEL, "ProgramArguments": command, "WorkingDirectory": str(project),
"RunAtLoad": True, "StartInterval": 3600, "ProcessType": "Background",
"EnvironmentVariables": {"PYTHONDONTWRITEBYTECODE": "1", "PYTHONUNBUFFERED": "1"},
"StandardOutPath": str(log_dir / "material_name_refresh.log"),
"StandardErrorPath": str(log_dir / "material_name_refresh.error.log"),
}
def main() -> int:
parser = argparse.ArgumentParser(description=__doc__)
parser.add_argument("action", choices=("install", "status", "uninstall", "preview"))
parser.add_argument("--python", type=Path, default=Path(sys.executable))
parser.add_argument("--kingdee-client", type=Path)
args = parser.parse_args()
if args.kingdee_client is not None:
args.kingdee_client = args.kingdee_client.resolve()
destination = Path.home() / "Library/LaunchAgents" / f"{LABEL}.plist"
logs = Path.home() / "Library/Logs/AM516_Feishu_Bot"
domain = f"gui/{os.getuid()}"
service = f"{domain}/{LABEL}"
if args.action == "preview":
print(plistlib.dumps(launch_agent(PROJECT_ROOT, args.python.resolve(), logs, args.kingdee_client)).decode())
return 0
if args.action == "status":
return subprocess.run(["launchctl", "print", service]).returncode
if args.action in ("install", "uninstall"):
exists = subprocess.run(["launchctl", "print", service], capture_output=True).returncode == 0
if exists:
subprocess.run(["launchctl", "bootout", service], check=True)
if args.action == "uninstall":
destination.unlink(missing_ok=True)
print("已移除物料名称后台刷新服务。")
return 0
destination.parent.mkdir(parents=True, exist_ok=True)
logs.mkdir(parents=True, exist_ok=True)
(PROJECT_ROOT / "logs").mkdir(exist_ok=True)
with destination.open("wb") as handle:
plistlib.dump(launch_agent(PROJECT_ROOT, args.python.resolve(), logs, args.kingdee_client), handle)
subprocess.run(["launchctl", "bootstrap", domain, str(destination)], check=True)
print("已安装物料名称后台刷新:每小时检查,成功刷新后间隔48小时再次查询 ERP。")
print(f"服务:{service}")
return 0
if __name__ == "__main__":
raise SystemExit(main())