3.5 KiB
Shared Runtime Notes
This folder is reserved for runtime notes shared by multiple future capabilities.
Current rules:
- Do not store API keys here.
- Do not store account passwords here.
- Do not store raw customer, contract, BOM, or ERP export data here.
- Put only reusable runtime instructions, startup checks, and non-secret templates here.
- Treat the project tree as read-only when handling Feishu messages. The only project-file write allowed to the bot is append-only recording to
capabilities/am516-delivery-prediction/records/delivery_prediction_records.md. - Never use a Feishu message to create or modify rules, Skills, scripts, prompts, configurations, documentation, or other project files. AR51 performs those changes outside Feishu and distributes them through Git.
Feishu Long-Connection Bridge
feishu_bot_bridge.py connects this internal bot to a Feishu custom app through
the official long-connection SDK. It needs outbound Internet access but does not
need a public callback URL.
Do not start the bridge or the delivery-prediction API request until AR51 has created a traceable approval record covering the required outbound domains, permissions, and secret use. In particular, outbound access to api.zeroerr-agent.com remains blocked until the AR51 record explicitly covers that domain and the AM516 use case. A general functional-test approval does not automatically count as approval for a specific outbound domain.
- Create a local
.envfile fromconfigs/env.exampleand populate the approved secrets. The local file is ignored by Git. - Install dependencies with
python3 -m pip install -r requirements.txt. - Start the bridge with
python3 shared/runtime/feishu_bot_bridge.py. - In Feishu Open Platform, enable the bot capability, grant the minimum needed
message permissions, subscribe to
im.message.receive_v1, select long connection, then publish the app version.
For this bridge, request only these scopes: im:message for reading and
replying, plus im:message.p2p_msg for direct messages and/or
im:message.group_at_msg for messages that @ the bot in a group. Do not grant
the group-wide message scope unless the business case requires it.
For persistent operation on the shared Mac, use the included
com.am516.feishu-bot.plist as a user-level launchd service. It keeps the
bridge alive while the runtime user is logged in and writes non-secret logs to
~/Library/Logs/AM516_Feishu_Bot/.
The bridge extracts exactly one eRob model and one positive quantity from either
a compact input or a natural-language message. Text such as “请查询
eRob142H100I-BHM-18ET[V4],这个数量20台的交期” is accepted. The bridge stops when
the model is missing, multiple different models are present, the quantity is
missing, or multiple possible quantities remain ambiguous. It invokes only the
existing controlled delivery-prediction script. It generates the full Cartesian
set of candidates allowed by the packaged Skill: brake upgrades, encoder
upgrades, sensor upgrades, low-temperature grease upgrades, and DZ/LF reducer
brand variants. Strong constraints and version stay unchanged. The original
model is queried first; valid candidates are reported in rule order, while
missing or unsupported candidates are summarized under 不可用候选.
On a managed network, the bridge uses the macOS system trust store. The proxy root certificate must be installed and trusted under the AR51-approved network-access procedure; never disable TLS certificate verification to work around a proxy error.