3.9 KiB
3.9 KiB
Deployment Checklist | AM516 Delivery Prediction
1. Account And Device
- Department shared Mac is confirmed as the runtime device.
- Device owner and reboot owner are confirmed.
- Department email is confirmed.
- Department ChatGPT / Codex account plan is confirmed.
- Account ownership, password custody, and handover method are confirmed.
- Screen lock, disk encryption, and remote management requirements are confirmed by AR51.
2. Git And Project
AM516_Feishu_Botis available on the shared Mac.- Git remote, branch, update, and rollback mechanisms are constructed by TH8.
- TH8 is the supporting IT department, but its project responsibility is limited to Git construction and excludes AM516 rules, functional implementation, network access, account permissions, secrets, and outbound approval.
- Branch and update method are confirmed.
- Mac Studio Codex has project write permission for AR51-assigned work through direct non-Feishu local entry points, including Codex automations or scheduled tasks and the required Git operations.
- The Feishu runtime account has read-only access to the project tree except append access to
records/delivery_prediction_records.mdand approved non-project log storage. - Project edits through Feishu are prohibited without exception; AR51-authorized rule and function changes are made outside Feishu and synchronized through Git.
- Permission checks distinguish the request entry point: Feishu requests do not inherit local Codex write permission even when Codex is the underlying executor.
- Rollback method is confirmed.
3. Secrets
- AR51 has approved the API-key purpose, storage, use, rotation, and revocation method in a traceable record.
ZEROERR_AGENT_API_KEYis configured without printing or committing it..envor local secret file is excluded by.gitignore.- No API key appears in Markdown, logs, Feishu output, or Git history.
4. Runtime
- Python 3 is available.
- The controlled script can run locally.
- AR51 has created a trusted approval record explicitly covering outbound access to
api.zeroerr-agent.com, the AM516 use case, and API-key use. - If that domain-and-permission record is absent, outbound access remains blocked; a general AR51 functional-test approval is not sufficient by itself.
- Only after approval is recorded, network can reach the AR836 delivery prediction API.
- Feishu bot bridge or local entry is configured.
- Logs are stored outside Git or in an approved non-secret location.
5. Acceptance
- AR51 confirms that AM516 rules, functional design, implementation, validation, iteration, network access, account permissions, secrets, and outbound approval are owned by AR51, not TH8.
- After the approval gate is satisfied, at least one valid model + quantity query succeeds; otherwise the blocked outbound state is recorded without attempting the request.
- Missing API key returns a structured error without leaking secrets.
- Missing, invalid, multiple, or ambiguous model/quantity input stays silent and makes no API call or record append.
- The initial response queries no more than four recommended candidates in addition to the original-model baseline; same-sender, same-chat continuation queries the next four without duplication.
- Candidate continuation without matching active context stays silent; a bridge restart or six-hour expiry requires the complete model and quantity again.
- Output includes the fixed internal-candidate disclaimer.
- Records append to
records/delivery_prediction_records.md. - A direct AR51 task in Mac Studio Codex can modify a test project file or perform the intended Git update without being blocked by the Feishu read-only rule.
- A Feishu request to modify a rule or other project file is refused and leaves all project files unchanged.