16 KiB
Acceptance Samples | AM516 Delivery Prediction
Use API-connected samples only after AR51 confirms the functional test and creates a separate trusted approval record explicitly covering api.zeroerr-agent.com, the AM516 use case, and API-key use. If that domain-and-permission record is absent, keep outbound access blocked and run only local, non-outbound checks.
Sample 1 | API Happy Path
Input:
eRob110H160I-FHM-18ET[V6] 10
Expected:
- model parses successfully;
- quantity is accepted;
- original demand 10 remains visible and each model is queried exactly once with quantity 10; stock accounting is handled by the API, with no local inventory deduction, yield adjustment or batch rounding;
- the bot immediately adds the Feishu
OnIt(typing) reaction to the original message after the valid trigger is accepted and before the API query starts; - the controlled script uses the macOS system trust store and keeps TLS verification enabled;
- the controlled script defaults to a direct HTTPS connection to
api.zeroerr-agent.com, ignoring system/environment proxies for this API only; it does not change Feishu or other applications' proxy settings; - an explicit
ZEROERR_AGENT_PROXY_MODE=systemuses the configured proxies; an invalid mode or a non-approved direct target stops before the request, and a failed request does not trigger an automatic proxy fallback or retry; - no temporary TLS-bypass parameter is required for the normal happy path;
- API script runs;
- output does not expose API key;
- output follows the successful-report field order in
skills/joint-module-leadtime-report/SKILL.md; - output includes old-format-style overall judgment, fastest candidate, coverage conclusion, numbered candidate details, recommendation reason, main factor, model difference, customer confirmation, and unavailable-candidate summary;
- output omits the
候选明细heading and does not repeat a human-review line under each candidate; - model differences use the compact
字段 原值→新值format and join multiple changes with;; - Feishu output uses rich-text
post; the report title, overall-judgment heading, numbered candidate headings, and unavailable-candidate heading are bold; - in initial and continuation replies, the
X个工作日and final delivery date values are bold in both最快候选交期and each model'sAM516预测交期, using native Feishu rich-text styles without displaying Markdown asterisks; - the judgment level and fixed disclaimer provide the global human-review boundary;
- inventory output is limited to summary-level available quantity and coverage; non-reducer shortage output never exposes material codes or raw ERP details;
- each usable model includes
缺料物料明细listing only shortage names, preserving order and deduplicating names; use the API's物料名称/缺料物料名称first, then resolve缺料物料throughdata/material_names.json; the same behavior applies to continuation replies; - code-only shortage records with cached names display those names without calling Kingdee; unresolved codes and missing/invalid caches are reported explicitly without displaying codes or inferring names; an empty shortage list says
API未返回缺料记录, and missing shortage data or invalid BOM keeps the unavailable-data reminder; - the cache is Git-trackable, contains only code/name mappings and source metadata, and works in another checkout without the source computer's paths or ERP credentials; refreshes with empty, invalid or conflicting data preserve the previous cache;
- the native background refresher queries ERP only when at least 48 hours have elapsed since the last successful refresh; unchanged dictionaries do not rewrite the Git cache, added/renamed names are merged, and failed refreshes preserve the cache and last-success state;
- running the updater on another computer uses that computer's local read-only ERP credentials, never Git-synchronized credentials; the bot sees valid cache changes on its next lookup without a restart;
- reducer shortages are the sole exception: when
缺料物料starts with20.30., output only the reducer code, inventory, inspection, in-transit, existing-demand quantities, and in-transit coverage conclusion in the Skill-defined order; - shortage items outside the
20.30.reducer prefix never expose their material codes or quantity details; - result is marked as internal candidate;
- all Skill-permitted brake, encoder, sensor, grease, and DZ/LF combinations are generated in a stable rule order without changing strong constraints or version;
- the original model is queried as a baseline and does not count toward the recommendation batch;
- the initial reply queries only candidate positions 1-4, details usable candidates, summarizes unsupported candidates under
不可用候选, states the remaining count, and invites the human to ask还有没有其他候选型号; - candidate position 5 and later are not queried or displayed in the initial reply;
- when the current four-candidate batch exceeds one Feishu rich-text message, it is split into ordered continuation posts and no candidate from that batch is dropped;
- record is appended.
- the appended record contains query metadata, model parsing, and a complete Markdown table with one row per model queried in the current batch;
- each future appended candidate row records the same query-completion time in
YYYY-MM-DD HH:mm:ss +0800form (with the actual local UTC offset), without rewriting or backfilling historical records; - record-table columns follow this order: 序号、记录时间、型号、推荐类型、差异项、API状态、AM516预测交期、可用库存、主导因素;
- unavailable candidates remain in their original rule order and are recorded as
❌ 不可用with unavailable result fields shown as—; lack of a result does not itself establish that the model does not exist;
Sample 1B | API Workdays And Final Delivery Date
Rules and expected results:
- read
data.交期汇总.AM516工作日交期anddata.交期汇总.AM516最终交货日期directly; - when the API returns
8and2026-10-08, outputAM516预测交期:8个工作日,最终交货日期:2026-10-08; - use the same workdays-and-date form in the fastest-candidate summary, initial and continuation candidate details, and newly appended record rows;
- ignore natural-day totals and the old
AM516预测交期field when selecting the displayed result; do not recalculate workdays or dates locally; - a valid API date in another calendar year remains usable without a local holiday calendar;
- accept zero workdays; reject negative, fractional, boolean, or non-numeric workday values and invalid dates;
- if either new field is missing or invalid, report the lead-time result as unavailable instead of falling back to old fields or estimating;
- a stopped original-model reply includes
原因:identifying each missing, empty, or invalid item in everyday Chinese and a suggestion to check the query result; no record is appended; - each unavailable candidate is listed with its own reason; HTTP 404 or missing fields must not be summarized as a confirmed nonexistent model;
- controlled-query failures explain their safe known cause in everyday Chinese, without HTTP codes, TLS, DNS, JSON, API Key, field-type requirements, arbitrary response bodies, or secret-bearing error strings;
- choose the fastest candidate using the API workday count, even when the natural-day totals would rank candidates differently.
Sample 1C | Product Model Not Found Notice
Local mocked response, matching AR51's screenshot:
{"success": true, "data": "产品型号不存在,请检查产品型号是否正确"}
Expected:
- for
eRob70H50I-FS-18CNC[V5], quantity 5, show查询系统提示:产品型号不存在,请检查产品型号是否正确。; - if this is the original model, stop before candidate queries and record append, with the reason and a plain-language suggestion to check the input;
- if this is a candidate, retain its batch position and show its own system notice under
不可用候选, for both initial and continuation batches; - do not show
data 格式错误or assume a delivery date fromsuccess=true; - unknown text and missing/unreadable query results must not be labeled as confirmed nonexistent models or echoed verbatim; explain the known issue in everyday Chinese;
- the fixed disclaimer appears once at the end, and no new dependency or configuration is required.
Sample 1A | Continue With Other Candidates
Preconditions:
- Sample 1 has completed in the same Feishu chat for the same sender;
- more than four rule candidates exist;
- the bridge has not restarted and the initial-query context is less than six hours old.
Input:
还有没有其他候选型号?
Equivalent inputs such as 还有吗、有没有别的、再推荐几个、继续、下一批
or more candidates must produce the same continuation behavior; exact wording
is not required.
Expected:
- the bot immediately adds the Feishu
OnIt(typing) reaction to the original message after the continuation and active-context gates pass; - the bot reuses the active model and quantity only for that same sender and chat;
- continuation retains original demand 10 and computes each new candidate from its own current stock; with zero stock production is 15. It never compounds an earlier adjustment or reuses baseline stock;
- the bot queries candidate positions 5-8 in the unchanged rule order;
- the original model and candidate positions 1-4 are not queried or displayed again;
- unavailable candidates still consume their original positions and are summarized under
不可用候选; - the reply states the current candidate range and the remaining count, or states that all rule candidates have been queried;
- one new record block contains only the models queried in this continuation batch;
- the fixed disclaimer appears once at the end.
If the same continuation text comes from another sender or chat, after a bridge restart, after the six-hour expiry, or without a valid initial query, the bot gives input guidance in private/relevant group messages, stays silent for unrelated group messages, and makes no API request or record append.
Unrelated expressions such as more interesting、继续查询英语例句、下一课 or
再来一首歌 do not qualify as candidate continuation, even while a query context exists.
Sample 2 | Missing Quantity
Input:
eRob110H160I-FHM-18ET[V6]
Expected:
- bot returns input guidance in private/relevant group messages; unrelated group messages stay silent;
- no acknowledgement reaction is added;
- no API call is made;
- no record is appended.
Sample 2A | Natural-Language Input
Input:
请帮我查询 eRob142H100I-BHM-18ET[V4],这个数量20台的交期,谢谢。
Expected:
- the bot extracts exactly one model:
eRob142H100I-BHM-18ET[V4]; - the bot extracts quantity
20from the surrounding natural-language text; - extra text does not cause rejection;
- the normal controlled-query and internal-candidate workflow continues.
Sample 2B | Ambiguous Natural-Language Quantity
Input:
请查询 eRob142H100I-BHM-18ET[V4],可能要20台,也可能要30台。
Expected:
- the bot identifies more than one possible quantity;
- the bot returns input guidance in private/relevant group messages; unrelated group messages stay silent;
- no API request is made and no record is appended.
Sample 3 | Invalid Model
Input:
eRob999X
Expected:
- bot returns input guidance in private/relevant group messages; unrelated group messages stay silent;
- no API call is made;
- no record is appended.
Sample 3A | Unrelated Group Message
Input:
这个机器人头像有点丑
Expected:
- bot stays silent for this unrelated group event; in private chat it returns usage guidance;
- no API call is made;
- no record is appended.
Sample 3B | Quantity Without A Complete Model
Input:
关节模组要10台
Expected:
- bot returns usage guidance in private chat; this group message without an eRob/AM516/交期/候选型号 keyword stays silent;
- no API call is made;
- no record is appended.
Sample 4 | Missing API Key
Condition:
ZEROERR_AGENT_API_KEY is not configured.
Expected:
- script returns a structured missing-key error;
- no secret is printed;
- bot reports environment incomplete.
Sample 5 | Project File Change Request
Input:
请修改 eRob 型号推荐规则,并写回项目文件。
Expected:
- bot returns input guidance because eRob is mentioned, but performs no project-file changes;
- no rule, Skill, script, prompt, configuration, documentation, or Git file is changed;
- no shell write, patch, editor, formatter, generator, or Git mutation command is run;
- the fixed delivery record file is not used to disguise or store a rule change.
Sample 6 | Default TLS Verification Failure
Condition:
- the normal controlled request encounters
CERTIFICATE_VERIFY_FAILED; --skip-tls-verifyis not supplied.
Expected:
- TLS certificate verification remains enabled;
- the script does not retry automatically or silently downgrade verification;
- the script returns a structured error identifying the local Python certificate-trust issue;
- the error states that an AR51-approved retry on a trusted network may use
--skip-tls-verify; - the error states that Python CA trust, the approved company proxy certificate, or the server certificate chain still requires a long-term repair;
- no API Key is printed or recorded.
Sample 7 | AR51-Approved Temporary TLS Retry
Preconditions:
- the normal request has failed with
CERTIFICATE_VERIFY_FAILED; - AR51 has explicitly approved one temporary retry;
- the Mac is on a trusted network;
- the target hostname is exactly
api.zeroerr-agent.com.
Input:
python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "eRob110H160I-FHM-18ET[V6]" --quantity 10 --skip-tls-verify
Expected:
- the script creates an unverified SSL context only because the flag is explicitly present;
- the context is passed to the request-local HTTPS handler used by the single controlled
opener.opencall; - the result does not expose the API Key;
- a successful response remains an internal candidate and requires human review;
- the temporary result does not remove the long-term certificate-repair requirement.
Sample 8 | TLS Bypass Requested For Another Host
Condition:
--skip-tls-verifyis supplied;- the configured target hostname is not exactly
api.zeroerr-agent.com.
Expected:
- the script stops before any outbound request;
- TLS verification is not disabled for the unapproved host;
- the script returns a structured hostname-guard error;
- no API Key is printed or recorded.
Required Final Disclaimer
以上为内部候选方案,不构成客户正式交期承诺;需 AR516 或授权责任人结合库存、生产、采购、客户优先级和最新系统数据人工复核后使用。
Original-Demand API Quantity Acceptance
- Regression:
eRob70F50I-FHM-18ET[V4] 12台, with API stock 10. Send quantity 12 once per model; show stock partly covering demand with a gap of 2. Preserve the API workdays/date and shortages. Do not show the old false-stock-branch error or calculate production 5 locally. - D=8/S=5: send 8; D=24/S=6: send 24; D=24/S=0: send 24; D=24/S>=24: still send 24 once and preserve the API response.
- Different candidates display their own stock, but all use unchanged original demand. Initial and continuation batches query each current-batch model once.
- Missing/invalid stock is unknown, never zero; valid API workdays/date remain usable with an explicit inventory-review item. Missing/invalid workdays/date or failed requests retain existing error handling.
- Initial and continuation Feishu reports show demand quantity, lead time and inventory coverage, but omit
数量传递规则,库存覆盖口径and per-modelAPI查询数量. Internal record metadata still contains actual API quantities and quantity rules. No local net-demand or production-quantity fields are shown. Historical records and existing candidate-table columns remain unchanged. - These checks use mocked responses locally. Runtime acceptance must verify actual API arguments and compare the displayed workdays/date with the same returned response; mocked dates do not constitute delivery predictions.