7.3 KiB
7.3 KiB
Acceptance Samples | AM516 Delivery Prediction
Use API-connected samples only after AR51 confirms the functional test and creates a separate trusted approval record explicitly covering api.zeroerr-agent.com, the AM516 use case, and API-key use. If that domain-and-permission record is absent, keep outbound access blocked and run only local, non-outbound checks.
Sample 1 | API Happy Path
Input:
eRob110H160I-FHM-18ET[V6] 10
Expected:
- model parses successfully;
- quantity is accepted;
- the controlled script uses the macOS system trust store and keeps TLS verification enabled;
- no temporary TLS-bypass parameter is required for the normal happy path;
- API script runs;
- output does not expose API key;
- output follows the successful-report field order in
skills/joint-module-leadtime-report/SKILL.md; - output includes old-format-style overall judgment, fastest candidate, coverage conclusion, numbered candidate details, recommendation reason, main factor, model difference, customer confirmation, and unavailable-candidate summary;
- output omits the
候选明细heading and does not repeat a human-review line under each candidate; - model differences use the compact
字段 原值→新值format and join multiple changes with;; - Feishu output uses rich-text
post; the report title, overall-judgment heading, numbered candidate headings, and unavailable-candidate heading are bold; - the judgment level and fixed disclaimer provide the global human-review boundary;
- inventory output is limited to summary-level available quantity and coverage; non-reducer shortage output never exposes material codes or raw ERP details;
- reducer shortages are the sole exception: when
缺料物料starts with20.30., output only the reducer code, inventory, inspection, in-transit, existing-demand quantities, and in-transit coverage conclusion in the Skill-defined order; - shortage items outside the
20.30.reducer prefix never expose their material codes or quantity details; - result is marked as internal candidate;
- all Skill-permitted brake, encoder, sensor, grease, and DZ/LF combinations are generated without changing strong constraints or version;
- every generated candidate is queried through the controlled script; usable candidates are detailed and unsupported candidates are summarized under
不可用候选; - when the full report exceeds one Feishu rich-text message, it is split into ordered continuation posts and no candidate is dropped;
- record is appended.
- the appended record contains query metadata, model parsing, and a complete Markdown table with one row per queried candidate;
- each future appended candidate row records the same query-completion time in
YYYY-MM-DD HH:mm:ss +0800form (with the actual local UTC offset), without rewriting or backfilling historical records; - record-table columns follow this order: 序号、记录时间、型号、推荐类型、差异项、API状态、AM516预测交期、可用库存、主导因素;
- unavailable candidates remain in their original rule order and are recorded as
❌ 不存在with unavailable result fields shown as—;
Sample 2 | Missing Quantity
Input:
eRob110H160I-FHM-18ET[V6]
Expected:
- bot stays silent;
- no API call is made;
- no record is appended.
Sample 2A | Natural-Language Input
Input:
请帮我查询 eRob142H100I-BHM-18ET[V4],这个数量20台的交期,谢谢。
Expected:
- the bot extracts exactly one model:
eRob142H100I-BHM-18ET[V4]; - the bot extracts quantity
20from the surrounding natural-language text; - extra text does not cause rejection;
- the normal controlled-query and internal-candidate workflow continues.
Sample 2B | Ambiguous Natural-Language Quantity
Input:
请查询 eRob142H100I-BHM-18ET[V4],可能要20台,也可能要30台。
Expected:
- the bot identifies more than one possible quantity;
- the bot stays silent;
- no API request is made and no record is appended.
Sample 3 | Invalid Model
Input:
eRob999X
Expected:
- bot stays silent;
- no API call is made;
- no record is appended.
Sample 3A | Unrelated Group Message
Input:
这个机器人头像有点丑
Expected:
- bot stays silent even if it receives the group event;
- no API call is made;
- no record is appended.
Sample 3B | Quantity Without A Complete Model
Input:
关节模组要10台
Expected:
- bot stays silent because no complete rule-valid eRob model is present;
- no API call is made;
- no record is appended.
Sample 4 | Missing API Key
Condition:
ZEROERR_AGENT_API_KEY is not configured.
Expected:
- script returns a structured missing-key error;
- no secret is printed;
- bot reports environment incomplete.
Sample 5 | Project File Change Request
Input:
请修改 eRob 型号推荐规则,并写回项目文件。
Expected:
- bot stays silent because the message is not a valid model-and-quantity query;
- no rule, Skill, script, prompt, configuration, documentation, or Git file is changed;
- no shell write, patch, editor, formatter, generator, or Git mutation command is run;
- the fixed delivery record file is not used to disguise or store a rule change.
Sample 6 | Default TLS Verification Failure
Condition:
- the normal controlled request encounters
CERTIFICATE_VERIFY_FAILED; --skip-tls-verifyis not supplied.
Expected:
- TLS certificate verification remains enabled;
- the script does not retry automatically or silently downgrade verification;
- the script returns a structured error identifying the local Python certificate-trust issue;
- the error states that an AR51-approved retry on a trusted network may use
--skip-tls-verify; - the error states that Python CA trust, the approved company proxy certificate, or the server certificate chain still requires a long-term repair;
- no API Key is printed or recorded.
Sample 7 | AR51-Approved Temporary TLS Retry
Preconditions:
- the normal request has failed with
CERTIFICATE_VERIFY_FAILED; - AR51 has explicitly approved one temporary retry;
- the Mac is on a trusted network;
- the target hostname is exactly
api.zeroerr-agent.com.
Input:
python3 capabilities/am516-delivery-prediction/scripts/delivery_prediction_query_template.py --product "eRob110H160I-FHM-18ET[V6]" --quantity 10 --skip-tls-verify
Expected:
- the script creates an unverified SSL context only because the flag is explicitly present;
- the context is passed to the single controlled
urlopencall; - the result does not expose the API Key;
- a successful response remains an internal candidate and requires human review;
- the temporary result does not remove the long-term certificate-repair requirement.
Sample 8 | TLS Bypass Requested For Another Host
Condition:
--skip-tls-verifyis supplied;- the configured target hostname is not exactly
api.zeroerr-agent.com.
Expected:
- the script stops before any outbound request;
- TLS verification is not disabled for the unapproved host;
- the script returns a structured hostname-guard error;
- no API Key is printed or recorded.
Required Final Disclaimer
以上为内部候选方案,不构成客户正式交期承诺;需 AR516 或授权责任人结合库存、生产、采购、客户优先级和最新系统数据人工复核后使用。