Files
AM516/shared/runtime/README.md

57 lines
3.8 KiB
Markdown
Raw Permalink Blame History

This file contains ambiguous Unicode characters
This file contains Unicode characters that might be confused with other characters. If you think that this is intentional, you can safely ignore this warning. Use the Escape button to reveal them.
# Shared Runtime Notes
This folder is reserved for runtime notes shared by multiple future capabilities.
Current rules:
- Do not store API keys here.
- Do not store account passwords here.
- Do not store raw customer, contract, BOM, or ERP export data here.
- Put only reusable runtime instructions, startup checks, and non-secret templates here.
- Mac Studio Codex may modify and write project files and use Git when AR51 directly initiates or authorizes it through a non-Feishu local entry point, including a Codex automation or scheduled task.
- Treat the project tree as read-only when handling Feishu messages. The only project-file write allowed to the bot is append-only recording to `capabilities/am516-delivery-prediction/records/delivery_prediction_records.md`.
- Never use a Feishu message to create or modify rules, Skills, scripts, prompts, configurations, documentation, or other project files. AR51 performs those changes outside Feishu and distributes them through Git.
- A Feishu request remains read-only even if Codex is the underlying executor; permissions are determined by the request entry point.
## Feishu Long-Connection Bridge
`feishu_bot_bridge.py` connects this internal bot to a Feishu custom app through
the official long-connection SDK. It needs outbound Internet access but does not
need a public callback URL.
Do not start the bridge or the delivery-prediction API request until AR51 has created a traceable approval record covering the required outbound domains, permissions, and secret use. In particular, outbound access to `api.zeroerr-agent.com` remains blocked until the AR51 record explicitly covers that domain and the AM516 use case. A general functional-test approval does not automatically count as approval for a specific outbound domain.
1. Create a local `.env` file from `configs/env.example` and populate the
approved secrets. The local file is ignored by Git.
2. Install dependencies with `python3 -m pip install -r requirements.txt`.
3. Start the bridge with `python3 shared/runtime/feishu_bot_bridge.py`.
4. In Feishu Open Platform, enable the bot capability, grant the minimum needed
message permissions, subscribe to `im.message.receive_v1`, select long
connection, then publish the app version.
For this bridge, request only these scopes: `im:message` for reading and
replying, plus `im:message.p2p_msg` for direct messages and/or
`im:message.group_at_msg` for messages that @ the bot in a group. Do not grant
the group-wide message scope unless the business case requires it.
For persistent operation on the shared Mac, use the included
`com.am516.feishu-bot.plist` as a user-level `launchd` service. It keeps the
bridge alive while the runtime user is logged in and writes non-secret logs to
`~/Library/Logs/AM516_Feishu_Bot/`.
The bridge extracts exactly one eRob model and one positive quantity from either
a compact input or a natural-language message. Text such as “请查询
eRob142H100I-BHM-18ET[V4]这个数量20台的交期” is accepted. The bridge stops when
the model is missing, multiple different models are present, the quantity is
missing, or multiple possible quantities remain ambiguous. It invokes only the
existing controlled delivery-prediction script. It generates the full Cartesian
set of candidates allowed by the packaged Skill: brake upgrades, encoder
upgrades, sensor upgrades, low-temperature grease upgrades, and DZ/LF reducer
brand variants. Strong constraints and version stay unchanged. The original
model is queried first; valid candidates are reported in rule order, while
missing or unsupported candidates are summarized under `不可用候选`.
On a managed network, the bridge uses the macOS system trust store. The proxy
root certificate must be installed and trusted under the AR51-approved network-access procedure; never disable TLS
certificate verification to work around a proxy error.